COVID-19 RECOVERY - Products and Solutions to help your business move forward - Learn More

Industry

Commercial

Improve Air Quality, Lower Energy Costs


Grainger Editorial Staff

Facility managers are in a bind. HVAC systems often use more energy than any other equipment or system in a building. According to the EPA, at least 45% of energy costs in commercial buildings are due to heating and cooling expenses. There’s even a tax rebate available, based on energy savings per square foot. And yet, if you reduce ventilation or turn the system off on weekends to save money, indoor air quality (IAQ) will worsen.

“I work in all kinds of buildings,” says Mike Klingler, service manager for Farber Corporation in Columbus, Ohio, “and I am often asked to reduce the energy costs of the HVAC systems. One of the areas we check is ventilation rates for the building.

Decreasing ventilation rates may reduce overall energy consumption and reduce operating costs but at the same time we have to maintain good indoor air quality standards too. There’s usually a very tight ventilation standard that the service provider has to control in order to reduce energy costs and maintain quality indoor air conditions. Considering the dynamic changes in a building and a functioning HVAC system, in many cases, it’s not real easy.”

Demystifying ASHRAE Standards and Indoor Air Comfort

Creating guidelines for “comfortable indoor conditions” has proven difficult due to the sheer number of variables—personal and environmental—that play a role in determining how people experience comfort. Similarly, good indoor air quality can be equally difficult to define as it largely depends upon the level of outdoor pollution, the number of occupants in any given space, or even an individual’s susceptibility to allergen or odor.

ASHRAE has developed two standards that address the subject of thermal comfort and ventilation: ASHRAE Standards 55 and 62.

ASHRAE 55 “Thermal Environmental Conditions for Human Occupancy” specifies the combination of environmental and personal factors that create a comfortable, productive environment for 80 percent of the occupants in any given space. The standard describes six primary factors that must be addressed when defining thermal comfort conditions: metabolic rate, clothing insulation, air temperature, radiant temperature, air speed, and humidity. These factors are considered in defining a range of operative temperatures that provide acceptable thermal conditions.

ASHRAE 62 “Ventilation for Acceptable Indoor Air Quality” defines the role that ventilation plays in the control of contaminants in the air. The standard specifies minimum ventilation rates and IAQ that would be acceptable to building occupants. Largely applicable to the design of new buildings, the standard is also intended for use as a guidance document to improve IAQ in existing buildings. A key consideration in the latest version of the standard (62.1-2004) is outdoor air quality, which is no longer ignored or assumed to be acceptable. These two standards actually suggest thresholds for all of the key parameters mentioned above. That makes ASHRAE a good source for optimizing HVAC systems to promote occupant comfort and, surprisingly, to manage energy costs.

How to Balance Your System

Once you know your thresholds, here are some tips for optimizing your HVAC system.

Proper Airflow—Conduct duct traverses to measure air pressure, velocity and flow. If pressure is too high and/or airflow too low, it could mean your system is working too hard to push too little air through. It’s probably time to replace dirty coils, fans and filters, which have probably been adding mold to the system, too.

Check Ventilation—Many buildings are either over-ventilated—needlessly spending energy on blowers—or under-ventilated, particularly airtight buildings built during the 1970s with underpowered ventilation systems. Under-ventilation leads to bad IAQ in a hurry. Use ASHRAE guidelines to get your balance just right.

Add Variable Frequency Drives (VFDs)The EPA recommends demand-based variable air volume systems, using VFDs to more efficiently regulate HVAC motors, pumps and so forth. That’s money up front for the installation but significant long-term savings in energy costs.

Temperature, Humidity and CO2—Regularly check indoor temperature, humidity and carbon dioxide levels, and compare them to the ASHRAE thresholds. Think of them as indicators, or hallmarks on your overall system health. If they’re in line, it’s likely that your system is well balanced and your tenants are happy.

In the end, HVAC energy costs are dictated by how often your equipment is working and how hard it has to work. Optimizing airflow stops equipment from overworking, while proactive pressure monitoring increases equipment lifespan. Controlling moisture (humidity) and contaminant infiltration in the building envelope promotes good indoor air quality, increasing productivity and reducing material and product damage.

And as Mike has found, “When I’ve got a big HVAC system and a lot of tenants, getting the balance right and checking it regularly can really help.”

The information contained in this article is intended for general information purposes only and is based on information available as of the initial date of publication. No representation is made that the information or references are complete or remain current. This article is not a substitute for review of current applicable government regulations, industry standards, or other standards specific to your business and/or activities and should not be construed as legal advice or opinion. Readers with specific questions should refer to the applicable standards or consult with an attorney.

SIGN UP FOR EMAIL

Get more great content like this sent to your inbox.

promo

THE PRODUCTS YOU NEED,
WHEN YOU NEED THEM

SHOP NOW